MOPOS

Latest Generation Drives for Turning Machines in the Box Malting Plant

Hops and malt – cold beer is almost essential for a gathering. The taste of the beer is determined by the malt that is added. Countless nuances of taste are created in a complex production process for which the machinery is in almost continuous use. One of the Czech Republic‘s leading manufacturers of malting equipment is Moravské Potravinářské Strojírny, abbreviated as MOPOS.

Focus on the Customer

Moravské potravinářské strojírny, a.s. Olomouc, abbreviated as MOPOS, is one of Europe's leading machinery manufacturers. In the food industry, the Czech company is regarded as a trend setter for state-of-the-art production lines and complete manufacturing plants, especially for the malting and bakery industries. Currently, more than 120 employees generate an annual turnover of more than 7 million dollars.

<h3>Focus on the Project</h3>
To cater to the special operating environment, MOPOS equipped the 8 turning machines of this malting plant with 112 parallel shaft gear units with smooth motors and 8 state-of-the-art drive units. The components are extremely well-protected against corrosion. The NORDAC PRO SK 500E series AC vector drives enable motor speeds which are matched to the various phases of the malting process.

Project Challenge

<h3>Hops and Malt</h3>

Cold beer is almost essential for a convivial gathering. The taste of the beer is determined by the malt which is added. Countless nuances of taste are created in a complex production process for which the machinery is in almost continuous use. One of the Czech Republic‘s leading manufacturers of malting equipment is Moravske potravinarske strojirny, abbreviated as MOPOS. For one of its customers, it replaced the malting plant turning machines and their drive units in 2015. During the entire production process the turning machines turn the grain in enormous troughs, so-called Saladin vats.

<h3>Stamina Required</h3>

Smooth operation of the malting process requires durable drive technology, because the malting process takes several days for each batch. The machinery is in continuous use for many years.

<h3>Production With Steam</h3>

The barley first has to be moistened so that it can germinate. The next step is a series of drying stages. This results in a production environment with a humidity of 100%. For operation at the condensation limit, the mechanical components require special corrosion protection and the electrical components require special insulation.

<h3>Acid-Resistant Housing</h3>

The carbon dioxide which is produced during drying can slow down the malting process. Because of this, it is extracted during drying. If it escapes into the operating environment it reacts with the steam. H<sub>2</sub>CO<sub>3</sub> is continually produced, which acts on the machines. NORD drive units with smooth, self-draining surfaces and special surface protection systems offer the ideal solution for such demanding production environments.

Application Solution

<h3>Weatherproof Equipment</h3>

The turning machines of the MOPOS malting plant are each equipped with 14 parallel shaft gear units. These were provided with a special surface treatment to ensure reliable operation in this special operating environment. This protects the smooth, ribless surface of the machinery against both the ambient atmosphere as well as against the high pressure jets of chemical cleaning agents, Thanks to the washdown design, these liquids drain off quickly and completely. The drives are protected with a high quality, chemical resistant paint system. Because they are installed vertically, the gear units only offer a small exposed surface.

The energy efficient NORD electric motors were designed with protection class IP66 to withstand the very high humidity; the temperature sensors and terminal boxes were encapsulated in resin and a moisture- resistant insulating paint protects the rotors and stators.

<h3>Stay Cool</h3>

The machine is moved by a 7 meter wide and more than 7,500 kg drive unit with multistage NORD parallel shaft gear units. This requires constant cooling. Due to the highly acidic humidity and the controlled movement of air for the process, fans were not an option. Instead, the drives are cooled entirely via their surfaces.

Thanks to a high reduction ratio in the gear units, the 8 turning machines travel at a moderate speed on rails above the 53 meter long and 2 meter deep malting troughs. NORD SK 500E series frequency inverters control the speed changes of the motors during the various phases of the malting process.

NORDAC PRO Variable Frequency Drive - SK 500E

Wide range of functions for cabinet control

  • Power Range: 0.33 – 200 HP (0.25 – 160 kW)
  • Protection Class: IP20
  • Flexibly Adjustable with Scalable Ethernet Interfaces
  • Scalable Range of Functions With Optional Plug-In Modules
  • Multiple-Axis Operation Controllable via Multi-Encoder Interface

UNICASE™ Parallel Shaft Gear Motor

Gearmotor with slim design

  • 0.12 kW – 200 kW
  • 110 Nm – 100,000 Nm
  • Slim design for space-saving installation
  • Wash-down capable, available with NXD tupH® for food-safe surface protection
  • Low noise thanks to quiet running

A6028 - Beverage industry


A6028 - Beverage industry
  • Download US-English
Documentation Details

A6033 - Food and beverage industry


A6033 - Food and beverage industry
  • Download US-English
Documentation Details

More Information